Technical FAQs

Ask a Question

Are NW scalable CAD drawings available?

NW scalable CAD drawings are available on CD # 48049-153-01 from the fulfilment center.

The dimensions for the 4 pole breakers would be an additional 4.53 inches for W-frame breakers and 9.06 inches for Y-frame.


CTA-ID : 2013296
Was this helpful?
What can we do to improve the information ?