Technical FAQs

Ask a Question

What is the maximum current rating available for the FUSIBLE Double Throw Safety Switches?

Issue:
Product Design Features

Product Line:
Double Throw Safety Switches

Environment:
Fusible switches

Cause:
Application

Resolution:
The maximum available current rating for a Fusible Double Throw Safety Switch is 100amps, at either 240Vac or 600Vac Max.




CTA-ID : 2013284
Was this helpful?
What can we do to improve the information ?