Technical FAQs

Ask a Question

Is an ATV38 AC drive available?

This is only available in Europe. Can use an ATV58 variable torque drive for North America. Base drive selection on the motor nameplate information and the application requirements.


CTA-ID : 2013092
Was this helpful?
What can we do to improve the information ?