Technical FAQs

Ask a Question

Is a connector furnished with a NEMA 12, 90 degree elbow?

A connector is shipped with the elbow as standard.


CTA-ID : 2013079
Was this helpful?
What can we do to improve the information ?