Technical FAQs

Ask a Question

What is the universal password for the Altivar 28?

Do not let just anybody know this password. This information is only to be used in emergencies. It is secret information. It may be best to attempt to have the drive replaced.

The universal password for the ATV28 is 6969. If an access code has been saved on the unit, this code will allow you to unlock the unit and program it. If the original code is unknown and no longer desired, remember to reset the Cod to 0 or to the desired code to be able to regain access.

CTA-ID : 2013075
Was this helpful?
What can we do to improve the information ?