Technical FAQs

Ask a Question

Does Schneider Electric offer a Flush mount version of the QO48M30DSGP or QO48M60DSGP Generator panel Load centers?

Issue:
Product design features

Product Line:
QO Load centers

Environment:
Flush mount covers

Cause:
Application

Resolution:
No, there are ONLY Surface versions available


 
Was this helpful?
What can we do to improve the information ?