Technical FAQs

Ask a Question

How do you wire ATV28 unit to run in forward and reverse directions?


Issue:   How do you wire ATV28 unit to run in forward and reverse directions?
 
Product Line:   ATV28
 
Environment:  All
 
Cause:   N/A
 
Resolution:   The factory setting of unit is 2-wire control which defaults LI1 terminal for forward direction and LI2 is factory default for reverse direction.
In order to have the unit run in either of these directions need to get 24v to the terminal desire to energize according to direction you want unit to run motor.


 
Was this helpful?
What can we do to improve the information ?