Technical FAQs

Ask a Question

Why does the ATV28 not operate off the keypad up and down arrow buttons to change speed and start unit?

This unit does not provide local control as standard allowing for change of speed reference and operation off keypad pad which is what is being described.  But to obtain this operation can use the part number VW3A28100 for the Local Operator Kit which has Run/Stop with Speed Potentiometer.


CTA-ID : 2013271
Was this helpful?
What can we do to improve the information ?