Technical FAQs

Ask a Question

How does the R3 operate on the ATS48 unit when set for tAI motor thermal alarm?

This is a NO normally open contact that when the unit reaches the set thermal state it changes the state.  This allows a signal to be sent out externally to alert that in thermal alarm before unit actually faults on this condition.


CTA-ID : 2013076
Was this helpful?
What can we do to improve the information ?