Technical FAQs

Ask a Question

What is the equipment ground bar kit used in the 400A and 600A heavy duty switches (ex. H365NR)?

Use PKOGTA2 (2 required if the ground wires are run in parallel)


CTA-ID : 2013074
Was this helpful?
What can we do to improve the information ?