Technical FAQs

Ask a Question

What is the suffix for 50 Degree C ambient rating on the FA/KA/LA/MA/NA frame circuit breakers?

Use the suffix 35 for 50 Degree C ambient rating (ex. FAL3610035)


CTA-ID : 2013069
Was this helpful?
What can we do to improve the information ?