Technical FAQs

Ask a Question

What is the heat dissipation for the ATV58HD46N4XZU drive at rated load?

This depends on the application:
For 40 HP Constant Torque applications, the dissipated power for this drive is 625 Watts at rated load.
For 30 HP Constant Torque Low Noise applications, the dissipated power for this drive is 561 Watts at rated load.
For 50 HP Variable Torque applications, the dissipated power for this drive is 770 Watts at rated load.
For 40 HP Variable Torque Low Noise applications, the dissipated power for this drive is 714 Watts at rated load.

See the installation guide for additional mounting instructions and guidelines.


CTA-ID : 2013259
Was this helpful?
What can we do to improve the information ?