Technical FAQs

Ask a Question

ATV28HU54N4U Why is there no hp rating listed?

This is a 3 kWatt 460V rated drive. The hp rating would fall between 3 hp and 5 hp. Can be used as long as the motor nameplate full load amps are not more than the drive output current rating of 7.1A.
There is no NEMA standard HP rating in this range. It is more common in Europe.

CTA-ID : 2013057
Was this helpful?
What can we do to improve the information ?