Technical FAQs

Ask a Question

Customer asks what size potentiometer goes with the RE7MY13MW

Customer was advised to see page 3 of the Zelio-Time Timer Catalog #9050CT0001 where it specifies that the Remote Control Input shall be linear at +/_ 20%, Resistance = 47Kohm +/_ 20%, Power = 0.2W, Maximum distance = 82` per shielded cable: shielding linked to terminal Z2.

CTA-ID : 2013696
Was this helpful?
What can we do to improve the information ?