Technical FAQs

Ask a Question

What is included in a 9998DRC12 contact kit?

Movable contact, stationary contacts, and screws. The movable contact is placed in one polybag, the stationary contacts are placed in another polybag, and the screws are placed in a third bag. These 3 bags are shipped in a carton.

CTA-ID : 2013694
Was this helpful?
What can we do to improve the information ?