Technical FAQs

Ask a Question

What is the replacement external reset mechanism for Series E 8538SBW22 combination starters?

The complete door mounted external reset mechanism assembly requires the following parts:

(1) 30019-114-90, reset subassembly.
(1) 30019-121-01, ring nut.
(1) 9066 W1, protective boot which serves as gasket and is required on NEMA 4X enclosures.


CTA-ID : 2013439
Was this helpful?
What can we do to improve the information ?