Technical FAQs

Ask a Question

What are the dimensions and the weight on the ATV58HD16M2XZU, ATV58HD23M2XZU, ATV58HD28N4XZU, ATV58HD33N4XZU and ATV58HD46N4XZU?

Width = 9.45 in (240 mm)
Height = 21.65 in (550 mm)
Depth is = 11.14 in (283 mm)
The weight is 75 lbs (34 kg)


CTA-ID : 2013256
Was this helpful?
What can we do to improve the information ?