Technical FAQs

Ask a Question

What is the recommended fuse size for the 230v ATV28 drives?

                               Class CC       Class J (1)
ATV28...
  U09M2U                10A                 10A
  U18M2U                15 A                15A
  U29M2U                20A                 20A
  U41M2U                30A                 30A
  U54M2U                25A                 25A
  U72M2U                30A                 30A
  U90M2U                ------                  50A
  D12M2U                ------                  60A
  D16N4U                 ----                  50A
  D23N4U                 ----                  60A

(1) Either fast acting or time delay Class J fuses can be used.


CTA-ID : 2013031
Was this helpful?
What can we do to improve the information ?