Technical FAQs

Ask a Question

What is the recommended fuse size for the 460v ATV28 drives?

                               Class CC       Class J (1)
  U18N4U                5 A                  5A
  U29N4U                10A                 10A
  U41N4U                10A                 10A
  U54N4U                15A                 15A
  U72N4U                15A                 15A
  U90N4U                30A                 30A
  D12N4U                 ----                  35A
  D16N4U                 ----                  50A
  D23N4U                 ----                  60A

(1) Either fast acting or time delay Class J fuses can be used.

CTA-ID : 2013030
Was this helpful?
What can we do to improve the information ?