Technical FAQs

Ask a Question

How can you get the ATV28 unit to run at high speed in the forward direction when only have a switch to start and stop unit?

When tCC (terminal strip control) is set to 2C (2-wire control) which is the factory default then HSP can be set to the desired speed would like to run the unit at.  Then with +10v jumpered to AI1 when you wire the switch between +24v and LI1 which is for the forward direction and it closes the unit will ramp up to high speed.


CTA-ID : 2013028
Was this helpful?
What can we do to improve the information ?