Technical FAQs

Ask a Question

How many skip frequencies is available to be programmed in the ATV58?

3 assignable jump frequencies are available - JPF, JF2 & JF3.
Each jump frequency has a bandwidth of +/- 2.5hz around JPF (jump frequency).

NOTE: Versions of the Altivar 58 before V4.1 IE 25 had only one available jump frequency. V4.1 IE 25 was introduced in the 3rd quarter of 2001.




CTA-ID : 2013025
Was this helpful?
What can we do to improve the information ?