Technical FAQs

Ask a Question

Do you have to use the EZML113225 with the EZM-TBU terminal boxes as stated in a footnote in the 173 digest?

The EZML113225 can be used with the EZM1800TB. The footnote in the 173 digest stating must be used with the EZM-TBU is incorrect.


CTA-ID : 2013237
Was this helpful?
What can we do to improve the information ?