Technical FAQs

Ask a Question

Can an additional 3 pole space be added to an existing 120/240 3 phase high-leg delta panelboard?

No, The number of 3 pole branches and spaces only must be specified when ordering. The B phase bus is insulated and all the connectors removed beyond the specified spaces and cannot be modified in the field.

CTA-ID : 2013228
Was this helpful?
What can we do to improve the information ?