Technical FAQs

Ask a Question

Is a watertight boot needed with a 9001KR for a NEMA4 application ?

NO ...the operator , itself , is NEMA4 rated . A boot is an optional


CTA-ID : 2013002
Was this helpful?
What can we do to improve the information ?