Technical FAQs

Ask a Question

What is Fault Close Current? What do I choose in the Product Selector?<br />

Fault close current is the maximum short circuit fault current a switch/device can close into and remain closed. Fault close currents are expressed in Asymmetrical amperes. Choose 12.5kA for Visi/Vac. 38kA is for 1200A HVL only and 25kA for HVL 600A and HVL/cc.




CTA-ID : 2013019
Was this helpful?
What can we do to improve the information ?