Technical FAQs

Ask a Question

Is Class 1 Division 2 (for explosive areas) classification available on any metal enclosed products?

Yes, the Class 1 Division 2 (for explosive areas) classification is available on HVL/cc switchgear 5kV - 17.5kV.

This is the only product with this rating. It is available in the Product Selector.


CTA-ID : 2013018
Was this helpful?
What can we do to improve the information ?