Technical FAQs

Ask a Question

Are different keys available for the XB6 keyed operators?

To order a key switch with a DOM311 key, add the suffix 1, also available with Ronis key numbers 201, 202 and 203 add the key number to the end of the reference. Example for key switch ZB6 AGB with Ronis key n*201 the reference becomes ZB6AGB201.

CTA-ID : 2013014
Was this helpful?
What can we do to improve the information ?