Technical FAQs

Ask a Question

At what frequency can you get nominal torque from the ATV28 drive?

Issue:   At what frequency can you get nominal torque from the ATV28 drive?
 
Product Line:   ATV28
 
Environment:  All
 
Cause:   N/A
 
Resolution:   You can get nominal motor torque at 1 Hz.


 
Was this helpful?
What can we do to improve the information ?