Technical FAQs

Ask a Question

Does Square D/SE offer Mechancial Key Interlocks for General Duty, Heavy duty and Double Throw Safety Switches?

Issue:
Product Design Features

Product Line:
Heavy Duty Safety Switches

Environment:
Factory installed Accessories

Cause:
Application

Resolution:
Mechanical Key Interlocks(or Key Interlocks) are available FACTORY INSTALLED ONLY for the Heavy Duty and Double Throw Safety Switches. But they are NOT available for the General Duty Safety Switches. For quoting information see the current on-line digest.


 
Was this helpful?
What can we do to improve the information ?