Technical FAQs

Ask a Question

For a CU12L400L, what are the replacement Nut & Washer for lug mounting on the studs, (6) total.

The part number for the lug mounting hardware is 40562-118-50. This is a baggie of 6 nuts and 6 flat washers.

CTA-ID : 2013212
Was this helpful?
What can we do to improve the information ?