Technical FAQs

Ask a Question

What is the spacing between the bus comb teeth on the following items:<br />MG10285<br />MG10286<br />MG10287

1 pole is 18mm which is also the space between the teeth.


CTA-ID : 2013007
Was this helpful?
What can we do to improve the information ?