Technical FAQs

Ask a Question

What is the NEMA rating of the XB6 operators?

They are rated NEMA 1, 4, 4X, and 12. Except for the keyed switches which are not NEMA 4X.


CTA-ID : 2013402
Was this helpful?
What can we do to improve the information ?