Technical FAQs

Ask a Question

What is the current rating of 8639 LTA4N softstart?

Issue: What is the current rating of 8639 LTA4N softstart?
 
Product Line: 8639 ATS46
 
Environment: All
 
Cause: N/A
 
Resolution: 480A.


 
Was this helpful?
What can we do to improve the information ?