Technical FAQs

Ask a Question

What is the current rating of 8638 or 8639 NRA4S, LRA4S, NRA4N or LRA4N and for the 8636 NRG4S, NRG4N, NRA4S or NRA4N soft starter.

Issue: What is the current rating of 8638 or 8639 NRA4S, LRA4S, NRA4N or LRA4N and for the 8636 NRG4S, NRG4N, NRA4S or NRA4N soft starter.
 
Product Line: Enclosed ATS46
 
Environment: 8638 8639 ATS46
 
Cause: N/A
 
Resolution: 361 amps.


 
Was this helpful?
What can we do to improve the information ?