Technical FAQs

Ask a Question

Does the Altivar ATV28 unit have Auto , Manual switching?

Issue:   Does the Altivar ATV28 unit have Auto , Manual switching?
 
Product Line:   ATV28
 
Environment:  All
 
Cause:   N/A
 
Resolution:   Yes, the unit does have Auto/ Manual switching which can be programmed in the I/O menu by assigning a LI (logic input) to rFc (reference switching).


 
Was this helpful?
What can we do to improve the information ?