Technical FAQs

Ask a Question

What are the dimensions and weight for ATV28HU41M2U, ATV28HU54M2U, ATV28HU72M2U, ATV28HU41N4U, ATV28HU54N4U, ATV28HU72N4U, ATV28HU41S6XU, ATV28HU72S6XU Altivar 28 drive?

Width = 5.6 in (140 mm) , Height = 7.8 in (195 mm), Depth = 6.5 in (163 mm)
The weight is 8.4 lbs (3.8 kg)

This information can be obtained in the ALTIVAR 28 Adjustable Speed Drive Controllers User`s Guide, Document Number: VVDED399062US



CTA-ID : 2013387
Was this helpful?
What can we do to improve the information ?