Technical FAQs

Ask a Question

What are the overall dimensions of the EZM1800CB?

ISSUE:
Product Design Features

PRODUCT LINE:
EZ Meter-Pak Metering Equipment

ENVIRONMENT:
Dimensions

CAUSE:
Installation

RESOLUTION:
The EZM1800CB is 53.97" Height x 18.66" Width x 11.50 inch depth. For all the dimensions see the below attached CAD drawing.


CTA-ID : 2013204
Was this helpful?
What can we do to improve the information ?