Technical FAQs

Ask a Question

What is the ambient temperature operating range for the ATV58 type N drives?

-10 to +40 *C (+14 to 104*F) without derating
-10 to +50 *C (+14 to 122*F) with derating of the current.
See the installation guide for additional details.

CTA-ID : 2013005
Was this helpful?
What can we do to improve the information ?