Technical FAQs

Ask a Question

Can ring type cable terminations be used with the 9070 Type T and TF Control Power Transformers?

Issue:
Transformer Termination Methods

Product Line:
LV Transformers

Environment:
Applies to LV Transformers by SquareD/Schneider Electric

Cause:
Ring terminals on Control Power Transformers

Resolution:

Yes, ring type terminations may be used on 9070 Type T and TF Industrial Control Transformers. The only exception to this is when the single terminal current rating exceeds the standard terminal capacity and special terminal block are supplied.


CTA-ID : 2013643
Was this helpful?
What can we do to improve the information ?