Technical FAQs

Ask a Question

Can we provide White interiors for HVL or HVL/cc?

Smyrna prefers to paint the low voltage wiring tub only for the white interior requirement. Use TAG #380.

If the entire enclosure must be painted white, the all enclosure parts have to be special make parts. This is not a preferred procedure.
Use TAG #297.


CTA-ID : 2013379
Was this helpful?
What can we do to improve the information ?