Technical FAQs

Ask a Question

What is the part number for the power board for the ATV66***M2S228?

This is a special power board and is obsolete no longer available.
This was a special drive that was made for Trane company. At the time that this was produced, there were no ATV66 drives made for 208/230 VAC input power. Altivar 66 drives ending in S228 were specially modified Altivar 66 460 VAC drives, adopted for 208-230 volt HVAC applications.

NOTE: The ``S228`` part numbers do not directly correspond to the ``M2`` part numbers. The dimensions and current ratings are not the same. Please verify correct current rating and dimensions before replacing these products with current ones.

CTA-ID : 2013090
Was this helpful?
What can we do to improve the information ?