Technical FAQs

Ask a Question

Customer needs to replace the XCKP contact block with gold flashed contacts.

Customer was advised that gold flashed contacts are not being offered anymore since fine silver contacts do as well.

The Standard fine silver contact block ( XESP2151) should be ok down to 5 volts DC @ 1mA.

CTA-ID : 2013198
Was this helpful?
What can we do to improve the information ?