Technical FAQs

Ask a Question

What do the suffix options on the Electronic Trip Unit STR55UP mean? (i.e.-F,T,R and C)

The definitions are as follows:
T: Residual type ground fault protection.
F: Fault indication.
R: load monitoring.
C: Communication with DIGIPACT.


CTA-ID : 2013196
Was this helpful?
What can we do to improve the information ?