Technical FAQs

Ask a Question

Customer asks how can he tell which are line and load lugs on the FVR high voltage breaker?

Customer was advised the C/T polarity is going to determine this. The convention is normally to have the H1 side of the C/T facing towards the source.

CTA-ID : 2012988
Was this helpful?
What can we do to improve the information ?