Technical FAQs

Ask a Question

Can a fixed NW breaker be converted to a drawout?

This cannot be done. Aside from fixing plates and primary connections, there are interlocks which cannot be adequately dealt with in the field. There is no repair or upgrade program in place. They will need to either use the fixed as a fixed or order a drawout.


CTA-ID : 2013189
Was this helpful?
What can we do to improve the information ?