Technical FAQs

Ask a Question

What is the range of the control voltage for the LH4N2**LY7?

The range for the control voltage for the LH4N2**LY7 units is 110V +10% -15% for terminals 06 & 07.

Unit rated below 25amps do not require external control voltage connection.


CTA-ID : 2012973
Was this helpful?
What can we do to improve the information ?