Technical FAQs

Ask a Question

What is the line frequency tolerance for the LH4N

The LH4N line frequency tolerance is 50/60 Hz (-10% / +15%).


CTA-ID : 2013600
Was this helpful?
What can we do to improve the information ?