Technical FAQs

Ask a Question

What type of motor thermal sensors can be used with the ATS48?

The total resistance of probe circuit should be 750 Ohms at 25 degrees C.
For example, three 250 Ohm probes in series


CTA-ID : 2012995
Was this helpful?
What can we do to improve the information ?