Technical FAQs

Ask a Question

What is the number for an AC auxiliarry switch for the ``SE`` type breaker?

Auxiliary switches catalog numbers are as follows;
4ac/dc = S34DCB2
4 ac/dc add on = S34DCT2
4 ac only = S34AC2
8 ac only = S38AC2


CTA-ID : 2012961
Was this helpful?
What can we do to improve the information ?