Technical FAQs

Ask a Question

Customer needs to replace the obsolete 9050FT12.

Customer advised that this electonic timer was unique because it had both instantaneous and timed contacts and +/-1% repeat accuracy. The 9050 Type A and B timers have both instantaneous & timed contacts but the repeat accuracy is +/- 10% and may not be acceptable as a replacement. End user must determine that.


CTA-ID : 2013182
Was this helpful?
What can we do to improve the information ?